AnsweredAssumed Answered

System Implementation ...

Question asked by inventis on Jan 22, 2010
Latest reply on Jan 25, 2010 by JeradL

Hello,

I'm writing the code for a microcontroller.

Reading the example in the "SYSTEM IMPLEMENTATION" chapert of the sigmastudio help I have some dubts:

 

In the example there is a To523 function

in this function a float value is converted and stored in an array with the array[0] the MSB and the array[3] the LSB.

 

In the example function SafeParam()

the array values computed with the To523 function seem to be inverded...

the sample code send array[4] .... array[0].

 

I'm a little confused.

Outcomes