AnsweredAssumed Answered

Linker error Blackfin 537 ???

Question asked by Sabin on Jan 7, 2010
Latest reply on Jan 11, 2010 by Sabin

I need help with one of the examples provided by analog devices that come with the book Wiley-Embedded Signal Processing with the Micro Signal Architecture.2007.The files compile but when it comes to linking several errors occur, all connected to the .ldf file.

 

First error is:

[Error el1010] ".\ALE.ldf":426 Parsing error: Invalid RESERVE command syntax: start address expression and alignment parameters are mutually exclusive.

 


The line where it points is:

RESERVE(___wab0=0xFFB00FFF - 75,___l0=76, 1) /* scratchpad */

 

And all lines where the "RESERVE" macro is used rise the same error.

The example is from the 4th chapter, experiment 4.4.

 

 

 

 

 

 

Thanks in advance.

Outcomes