AnsweredAssumed Answered

UART example which works with RTS/CTS handshaking

Question asked by Milos on Dec 22, 2009
Latest reply on Dec 22, 2009 by Milos

Hello,


I’m looking for UART example which works with RTS/CTS handshaking?

There is “UART Echo Back” but it doesn’t work with RTS/CTS.

 

Especially, I’m looking for pin definition for RTS and CTS and register settings for hardware flow control.

 

something like this

SRU2(UART0_TX_O,DPI_PB09_I); // UART transmit signal is connected to DPI pin 9

  SRU2(HIGH,DPI_PBEN09_I);

  SRU2(DPI_PB10_O,UART0_RX_I); // connect the pin buffer output signal to the UART0 receive

  SRU2(LOW,DPI_PB10_I);

  SRU2(LOW,DPI_PBEN10_I);      // disables DPI pin10 as input

 

Thanks,

Milos


Outcomes