AnsweredAssumed Answered

External SDRAM doesn't work on 96kHz...

Question asked by ChLatte on Nov 10, 2009
Latest reply on Nov 24, 2009 by CraigG

hi....

 

when I link my project (reverberation via SIMULINK embedded IDE link) it works fine on 48kHz, but when I try it on 96kHz it only talks thru...

thats why the data section for reverberation is on SDRAM....because for internal on-chip memory it is too large..

 

an other problem is that I try hard to flash the project....I use the default PROM > hex > 8bit > .ldr and flash it with the flash programmer successful...but it don't consider the SDRAM

 

 

see attachment for linker file..............

Attachments

Outcomes