AnsweredAssumed Answered

AD8317 output voltage dispersion at high frequencies

Question asked by bcampag Employee on Oct 26, 2009
Latest reply on Oct 26, 2009 by enash

In the datasheet of the AD8317, the min and max values of the output voltage for input power of -10 and -40dBm are given for 900MHz, but not for higher frequencies.

I would like some distribution information of the output voltage for Pin= -10 and +40dBm and Fin= 7GHz, 7.5GHz, 8GHz and 8.5GHz.

I understand that some data can be found in the graphs and that we will not garantee min/max values, but any table of data close to this request will be usefull.

Thanks

Bertrand

Outcomes