AnsweredAssumed Answered

shell_browser example: supported USB Flash drive

Question asked by vix on Oct 20, 2009
Latest reply on Jan 17, 2012 by CraigG
Branched to a new discussion

I recompiled and built the supplied shell_browser example for BF527, then I tried with 3 different USB Flash devices:

  1. 256MB - FAT filesystem              works
  2. 512MB - FAT filesystem              doesn't work
  3. 512MB - FAT32 filesystem          doesn't work


For the devices not working, the event ADI_USB_EVENT_RX_COMPLETE in HostEndpointZeroCompleteCallback( ) function doesn't happen.

Could someone give me some help on this problem?

Are there any additional modifications to the supplied example to have all the USB Flash devices working?

Is there any problem if size is greater than 256MB or filesystem not FAT?

Outcomes