AnsweredAssumed Answered

AD7794 occasional spikes

Question asked by PeterT on Jun 13, 2013
Latest reply on Jun 14, 2013 by J.Gealon

Hello,

 

I am using an AD7794 in an application where I measure resistances. When acquiring many consecutive samples in continuous  mode I see occasional spikes ( every couple of 10000 samples) in the signal which I attribute to the ADC. Please see the attached plot. The discretization in the plot comes from formating the output to 3 decimal places.

 

The setup is as follows:

 

*  for circuit see attachment

*  DIN is tied high between write operation

*  SCLK  is high in the idle state

*  Sample rate 470 Hz

*  continuous  mode

*  external (ratiometric) reference

 

Any advice on what might cause this effect ?

 

Thank you and best regards

Peter

 

 

 

UPDATE:

I seem that the spike were due to a very noisy TTL RS232 converter IC .... after switching it off during ADC the spikes disappeared ...

Attachments

Outcomes