AnsweredAssumed Answered

Internal resister for ADG465

Question asked by Kaos on Jun 11, 2013
Latest reply on Jun 13, 2013 by Kaos

Dir Sir/Madam,

 

I have some questions for ADG465BRTZ.

 

Question-1
Does the following 2 functions same as MUX ADG508F and ADG509F?

1)Over voltage protection
2)When power off, the internal MOSFET D-S keep off

 

Question-2
When ADG465 is out the following conditions, what is the internal resistance?

case-1:input signal=non(0V)
case-2:input signal=5Vdc

 

Question-3
When the supply power is off, what is the internal resistance?
I think that the internal resistance show over 10Mohm.

Please explain these.

 

Thanks Kaos

Outcomes