AnsweredAssumed Answered

VisualDSP++ editor can work with max 2049 characters in one row

Question asked by Afinko on Oct 16, 2009
Latest reply on Oct 16, 2009 by Afinko

If I want to add more than 2049 characters in one row, the VisualDSP++ editor automatically disassembly the row in more rows with 2049 characters.

However, in this case, the compiler take the next row as a new line, and mostly produce an error.

 

Is there a way how to set the editor to work with larger row than 2049?

Is there some special character, that I can add at the end of the row so the compiler will take new row as the same line?

 

Thanks,

Afi

Outcomes