AnsweredAssumed Answered

Migrating Blackfin BF527 to BF524

Question asked by vito on Jun 10, 2013
Latest reply on Jun 12, 2013 by CraigG

Hi,

 

I have a project for BF527, but I'm having some issues with USB and decided to move to BF524.

Once I have updated Project options to BF524 (all other options are set as in original BF527) - I'm

getting problems with adi_ssl_init.c. What is causing those & how to solve?

 

Thanks a million,

Rgds,

vito

 

 

"..\..\..\hal\adi_ssl_Init.c", line 544: cc0020:  error: identifier

          "asynch_bank_trans_time" is undefined

          { ADI_EBIU_CMD_SET_ASYNCH_BANK_TRANSITION_TIME,   (void*)&asynch_bank_trans_time  },

                                                                    ^

 

 

"..\..\..\hal\adi_ssl_Init.c", line 545: cc0020:  error: identifier

          "asynch_bank_read_access_time" is undefined

          { ADI_EBIU_CMD_SET_ASYNCH_BANK_READ_ACCESS_TIME,  (void*)&asynch_bank_read_access_time  },

                                                                    ^

 

 

"..\..\..\hal\adi_ssl_Init.c", line 546: cc0020:  error: identifier

          "asynch_bank_write_access_time" is undefined

          { ADI_EBIU_CMD_SET_ASYNCH_BANK_WRITE_ACCESS_TIME, (void*)&asynch_bank_write_access_time  },

                                                                    ^

 

 

"..\..\..\hal\adi_ssl_Init.c", line 547: cc0020:  error: identifier

          "asynch_bank_setup_time" is undefined

          { ADI_EBIU_CMD_SET_ASYNCH_BANK_SETUP_TIME,        (void*)&asynch_bank_setup_time  },

                                                                    ^

 

 

"..\..\..\hal\adi_ssl_Init.c", line 548: cc0020:  error: identifier

          "asynch_bank_hold_time" is undefined

          { ADI_EBIU_CMD_SET_ASYNCH_BANK_HOLD_TIME,         (void*)&asynch_bank_hold_time  },

                                                                    ^

 

 

"..\..\..\hal\adi_ssl_Init.c", line 549: cc0020:  error: identifier

          "asynch_bank_ardy_enable" is undefined

          { ADI_EBIU_CMD_SET_ASYNCH_BANK_ARDY_ENABLE,       (void*)&asynch_bank_ardy_enable  },

                                                                    ^

 

 

"..\..\..\hal\adi_ssl_Init.c", line 550: cc0020:  error: identifier

          "asynch_bank_ardy_polarity" is undefined

          { ADI_EBIU_CMD_SET_ASYNCH_BANK_ARDY_POLARITY,     (void*)&asynch_bank_ardy_polarity },

                                                                    ^

 

 

7 errors detected in the compilation of "..\..\..\hal\adi_ssl_Init.c".

cc3089: fatal error: Compilation failed

Tool failed with exit/exception code: 1.

Build was unsuccessful.

 

 

Rgds,

vito

Outcomes