AnsweredAssumed Answered

MHL / HDMI to V-by-One

Question asked by pdanders on Jun 3, 2013
Latest reply on Jun 4, 2013 by DaveD

Hello,

I'm in need a circuit that can take HDMI (specifically MHL from a  cell phone) and translate it to V-by-One.  From what I can tell V-by-one  is only supported by Thine so what I need is HDMI to bus X and then use  the Thine THCV213 transmitter to go from bus X to V-by-one.

http://www.thine.co.jp/products_e/V-by-One/

 

What I'm struggling with is Bus X.  It's a 18 bit parallel data bus.   I'm sure it's a standard but I can't seem to figure out what it is or  the bus is something I found with fewer bits like RGB which sounds like  there are 3 8 bit busses.  So does Analog have anything to convert HDMI into  a interface compatible with the Thine transmitter?  Is the Thine input  bus a standard?

Ideally, I'd like to support multiple inputs but HDMI/MHL is #1.

The display is a 800x600 8" touch screen LCD. 

 

Any help would be appreciated.

Outcomes