AnsweredAssumed Answered

adv212, precision of image

Question asked by condone on Jun 2, 2013
Latest reply on Jun 3, 2013 by DaveD

hi,

 

I'm using adv212 to encode still image now. The interface mode is HIPI. I notice that the option of encode firmware parameter PREC (Program Guide, pp 43) is 8-bit, 10-bit, and 12-bit. However, in User's Guide, option of PREC in PMODE1 register is 8-bit, 10-bit, 12-bit, 14-bit and 16-bit. So can adv212 encode image with precision more than 12-bit, e.g. 14-bit or 16bit? If the answer is yes, how should i configure the firmware parameter?

 

BR.

Tiandong Wang

Outcomes