AnsweredAssumed Answered

AD2S1210 Dynamic Performance

Question asked by Osamu on May 30, 2013
Latest reply on Jun 12, 2013 by J.Gealon

Hello.

 

I have a question about Dynamic Performance.

Dynamic performance has 1200Hz ~ 2200Hz when 3.192MHz clock in and 12bit.

This is the spec of 10kHz ~ 20kHz external frequency.

So, if that is fixed to 20KHz or 10kHz of external  frequency, how much will be the frequency of the dynamic response .

Outcomes