AnsweredAssumed Answered

ADXRS453 Temperature Sensor

Question asked by Alexspin on May 29, 2013
Latest reply on Jun 26, 2013 by venkat

Hi all,

We're developing a system that used ADXRS453. We connect the evaluation board (EVAL-ADXRS453Z-V) at our acquisition system and read the sensor at rate of 1kHz (the sampling rate of the sensor is about 485Hz, so we have 2 sample with the same value).

First of all we have analyzed the temperature information in order to check the communication. The result is shown in the attached image.

Temperature.jpg

The communication seems to be correct, it returns no errors, and the parity is checked.

 

 

Thanks for your help.

Alex.

Outcomes