AnsweredAssumed Answered

Max channel number of sharc 21488's TDM.

Question asked by Ares on May 27, 2013
Latest reply on Jun 17, 2013 by jeyanthi.jegadeesan

Hi,

 

For 21488, I have a question about maximum channel number of a specific SPORT, let's use SPORT0 as an example,

if SPORT0_CLK is 12.288MHz, sample rate is 48kHz, and word length is 32bit, so in TDM multichannel mode, the maximum channel number is

12.288M / 32 * 48k = 8 channels, if both SPORT0's DA and SPORT's DB data line are used, the maximum channel is still 8 channels or 8 x 2 (DA and DB) = 16 channels?

 

Thanks in advance!

Outcomes