AnsweredAssumed Answered

2012R2-RC5 Buildroot bf537-stamp x86_64 compilation problem with external toolchain

Question asked by dbueno-baques on May 23, 2013
Latest reply on May 24, 2013 by dbueno-baques

Hi everybody:

 

I'm trying to make an initial image out of buildroot 2012R2-RC5 for a bf537-stamp (toolchain 2012R2-RC2.x86_64 and same for uclibc-full), but seems that something is wrong. Follows the command sequence and error:

 

1. make bf537-stamp_defconfig => OK!

2. make => error

 

.....

checking for bfin-uclinux-gcc... /home/dbueno/Equip/blackfin-buildroot/output/host/usr/bin/bfin-uclinux-gcc

checking for C compiler default output file name... configure: error: C compiler cannot create executables

See `config.log' for more details.

make: *** [/home/dbueno/Equip/blackfin-buildroot/output/build/gdbserver-6.6a/.configured] Error 77

 

I would really appreciate any hints, solutions, commentaries!!!

 

D. Bueno

Outcomes