AnsweredAssumed Answered

How to read in ADSP-BF51x .ldr file one byte at a time?

Question asked by jimhi on May 22, 2013
Latest reply on May 23, 2013 by Andreas

I have a ADSP-BF51x with the ADSP-BF518F EZ-Board. I am booting it through SPI Slave Boot mode, but according to the specs I have to check if the HWAIT Pin is low after sending every single byte. Is there a way to convert the loader file into an array of unsigned chars so I can do this in c++?

 

A link to an example would help. Also, once the last byte is sent through SPI, it should run whatever file I just sent it correct?

 

Thanks.

Outcomes