AnsweredAssumed Answered

Connecting serial data to other ICs in Sigma App

Question asked by chuckwin on May 22, 2013
Latest reply on Jun 13, 2013 by chuckwin

Hello,

 

I have 3 ADAU1761's in a single project. Design requirements call for summing of 3 signals into a single output. I have made this work already on a shipping product by daisy chaining sdataout1 to sdatain2,  sdataout2 to sdatain3, and performing the sum of 1,2&3 in IC3.

 

What I'd like to do is to be able to connect them in the Sigma schematic so I can  assure myself the right signals are being combined.

 

Failing that, is there a way to draw lines on the schematic to indicate the source and destination of each serial port?

 

Thanks for any help you can offer.

 

sincerely

chuckwin

Outcomes