AnsweredAssumed Answered

UART Overrun Error

Question asked by NTan on May 22, 2013
Latest reply on Jun 10, 2013 by Andreas

Good Day Everyone!

 

I'm trying to interfaace a serial camera to the UART1 of a BF537 EZ Kit Lite. I've edited the uart library included in EE-347. However, I keep getting overrun error right after initializing UART (UartInit function).

 

I have already switched off SW5.1 and SW5.2 and I have also connected the TX pin of the camera to the RX pin of UART1 (pin 10) and the RX pin to TX pin of UART1 (pin 6).

 

When I remove the connection from pin 10 (RX), initialization works and there is no error. However, when I return the connections to pin 10, Overrun error occurs right after initialization.

 

What may be the problem? I have attached my code here...

Attachments

Outcomes