AnsweredAssumed Answered

I need adv7511 transmitter API source codes

Question asked by mugox on May 17, 2013
Latest reply on May 28, 2013 by DaveD

Hi all,

 

I am trying to use AD7511 on the AC701 xilinx development kit. There are some example projects in http://wiki.analog.com/resources/fpga/xilinx/kc705/adv7511. But all of them are microblaze based. Because of the licencing and some other problems, I dont want to use microblaze. So I have to port the microblaze code to TI MCUs. I see there are some APIs(called ADV7511 Transmitter API) that are used for AD7511 init and use. APIs are well defined in http://wiki.analog.com/resources/fpga/xilinx/adv7511 and in some pdfs. But since I have to port the APIs, I need source codes of the library (libHDMI_MicroBlazeLib.a). The examples are GitHub based and open source. So the source code of the API must be somewhere in there. But I couldn't find.  Could you please help? 

 

Best.

Outcomes