AnsweredAssumed Answered

Wireless communicaton of video and image b/w DSP and PC

Question asked by m.Abdullah on May 16, 2013
Latest reply on May 28, 2013 by SachinV

Hi Sir,

I am student of undergrad. The title of discussion is my final year project. i have following hardware:

1. ADSP-BF561 EZ - Kit lite

2. Jmk-JK-307 (CMOS sensor)

 

i m using VDSP++ 5.0 for coding. i tried the example code of video talk through of BF561 name as "Video Input-Output (C)". i connected the video source at video input (J6) via AV cable. i also connected the monitor via AV cable at video output (J6). when i ran the example code i got the output at monitor.

now i want to send the video wirelessly at approx 200m range PC. now there are two ways for me to send it.

1. through wifi module

2. wireless transmitter

 

i started working on wifi module. for this purpose i have to code SPI, because the wifi module named as "EasyWiFi" of MikroElectronica

has SPI port to be connected. the problem is i don't know where to write the code for SPI to connect the Wifi Module with kit. kindly help me regarding this.

 

and also tell me if i connect the wireless transmitter at the video output (J6) via AV cables, it will work or not?

for details of Wifi, camera and wireless transmitter/ receiver links are given below.

 

for wireless TX/ RX: http://www.alibaba.com/product-gs/252479115/2_4GHz_400mW_Wireless_AV_Transmitter.html

for Camera : http://alnect.net/products.php?/13/88/263/1059/Special-Tools/CCTV-IP-Camera/Wired-CCTV-Camera/Kamera-CCTV-Indoor-Mini-Type-JMK-JK-307A

for wifi module the afile is attached. i am waiting for help.

 

regards,

Adullah

Attachments

Outcomes