AnsweredAssumed Answered

ADV7619-7511 eval board read/write registers

Question asked by snageli on May 15, 2013
Latest reply on May 20, 2013 by GuenterL

I am trying to read and write registers over the serial port to the ADV7619 on the ADV7619-7511 eval board.  I have used the help command to see what all the available commands are. 

 

For 'wri2c' and 'rdi2c' it shows that the command should be structured as follows:

 

example - rdi2c <device> <address>

 

what should the <device> be in the case of the ADV7619, should it be adv7619 or just 7619?  I have tried several iterations but all I get back is that it read a 0 for any address I read.  I am also doing as instructed and not placing a 0x in front of the address.

 

Thanks,

Outcomes