AnsweredAssumed Answered

ADL5375 Switch DP4T

Question asked by Zartagal on May 14, 2013
Latest reply on Jun 17, 2013 by THA

Hi!

I'm working with a new design based on the ADL5365 modulator and the ADL5380 demodulator. They both can reach a frequency of 6 GHz. The LO input is a differential-one. I'd like to use two different filters in the input to reject the armonics for two different bands like it's described in the CN-0134 application note (p.5).

There is proposed to use a DP4T switch to conmutate between the two paths. My circuit needs to use the hole range, up to 6GHz and I would need a switch with this frequency range too.

Could you recommend me a device to comply with this specifications?

 

Thanks in advance,

Regards

 

G. Asencio

Outcomes