AnsweredAssumed Answered

interfacing arduino uno with ad9834

Question asked by anasch on May 10, 2013
Latest reply on May 10, 2013 by musach

Hi

I want to interface an arduino uno with eval ad9834 board i make these connexion it is true or not

Sdata ====> pin 12

Sclk =====> pin 10

Fsync =====>pin 11

Dvdd ====> 5V

Dgnd ======>GND

(SPI: 10 (SS), 11 (MOSI), 12 (MISO), 13 (SCK). These pins support SPI communication for arduino uno )

 

and i try to use this code to generat a single signal :http://ez.analog.com/message/31967#31967

but no result

Outcomes