AnsweredAssumed Answered

1701 INPUT OUTPUT HALF

Question asked by Sojourney on May 9, 2013
Latest reply on May 15, 2013 by audiolab1

hi, everyone,

i have a test about 1701, analog input,  after the L/R ADC input Resistance 18k, the signal, reduce to 1/2 RCA input level.

like ADC input 1.0V,  test the point after Resistance 18k, just have 0.5V, and the DAC output also have 0.5V,  but inside the DSP is do nothing, just passthrou.

 

when i put a Gain function inside the DSP, like +6dB, and then the DAC output have 1.0V, but have noise. i didn't have check if output is clip.

any ideas ?

Outcomes