AnsweredAssumed Answered

Cross compile error...

Question asked by s3283661@student.rmit.edu.au on May 8, 2013
Latest reply on May 10, 2013 by s3283661@student.rmit.edu.au

Hi,

    I really need some help for cross compilation as I am try to compile Pocketsphinx on to BF 548 EZ-KT. When I run my own compile version, it shows this error on the blackfin console:

  

ad_oss.c(103): Failed to open audio device(plughw:0,0): No such file or directory

FATAL_ERROR: "continuous.c", line 246: Failed to open audio device

 

    I have been following "Cross Compiling Applications" in the quick start guide ( http://docs.blackfin.uclinux.org/doku.php?id=quick-start:bf548-ezkit ). I am using the Blackfin live DVD provided and Pocketsphinx-0.8. There is a pre-compile demo of Pocketsphinx in the DVD. When I run the demo, the program works perfectly. But when I run my own, it shows the error above. I think uClinux distribution is set correctly. Should be somewhere wrong with the host environment or the command.

 

  Please help me with this problem. Thanks a lot.

 

Kind regards,

Wen

Attachments

Outcomes