AnsweredAssumed Answered

ADF4110 Channel Spacing

Question asked by YSVenu on May 3, 2013
Latest reply on Oct 27, 2015 by rbrennan

Hi,

 

I am using the ADF4110's N Counter with the Dual Modulus Prescalar as a Programmable Divider. The input frequency from the VCO varies from 1MHz to 32MHz (square). I should produce a 500Hz output from the ADF4110 at phase locked condition at all frequencies.

 

1. The input square wave has an amplitude of 2V. I need to square up the input as sharp as possible to achieve the slew rate required by the ADF4110's input. Please suggest a good comparator that would do the same...?

 

2. The Channel spacing of my system is 1KHz. Could I achieve this through the ADF4110 at all input frequencies...?

 

Regards,

YSVenu

Outcomes