AnsweredAssumed Answered

ADV7525/6  VIC code issue

Question asked by sviengkhou on Apr 30, 2013
Latest reply on May 2, 2013 by DaveD

Hello ,

I’m using the ADV7525 and I see that when the input video is HD 720p@59.94/60Hz the reported vic code is 0 instead of 4 on register 0x3e.

The video output is fine, but why is the Vic code not correctly reported.   I get this issue with these formats:

 

HD/1080p/24=00h (No Video Code in AVI infoframe)

HD/720p/60=00h (No Video Code in AVI infoframe)

 

My source is a CEA-861 compliant Phabrix.

 

Regards,

SV

Outcomes