AnsweredAssumed Answered

AD1934 data bits per channel is only 32bits in single-line DAC TDM or Dual-Line DAC TDM?

Question asked by yunchangxiao on Apr 27, 2013
Latest reply on Jul 18, 2013 by ColemanR

Single-Line.pngDual-Line.pngdata.png

QUESTION:

1.If I configue the AD1934 in single-line DAC TDM or Dual-Line DAC TDM,per channel must have 32bits??? I use the BF518 to control the ad1934 in multchannel mode. So I have to configure the sport transmit 32bits per channel?

2. Could I configure the TDM mode in 16bits per channel through the DAC Control 2 register. And the word width of this register is only for I2S mode???

3.Whether the 32bits  means per channel has the maximum bits is 32?

Outcomes