AnsweredAssumed Answered

How to set the coreB start address in CCES

Question asked by HoJuly on Apr 26, 2013
Latest reply on Apr 29, 2013 by StuH

Hi!

    I have combined u-boot and BF609_MCAPI_msg_CORE1.dxe as "test_mcapi.html" said: use the below command, and set boot-mode to nor flash to start the system.

 

bfin-elf-ldr -T bf609-0.0 -c DualCoreTest_uboot.ldr u-boot BF609_MCAPI_msg_CORE1.dxe --bmode PARA --use-vmas --initcode arch/blackfin/cpu/initcode.o  -J --punchit $((0x8000)):$((0x8000)):env-ldr.o

 

In CCES, the setting is:

66a50225.bmp

Does "Internal memory" means:  CORE1.dxe running from L2 SRAM?  ------The size of L2 SRAM in BF609 is 256kB, Will CORE1.dxe fail to start If the code size of CORE1.dxe is bigger than 256kB ?

 

If I set "Internal memory" to "custom 0x0700 0000"(In bf609-ezkit, the size of DDR2 is 128M), Will CORE1.dxe start at the place in DDR2?

Outcomes