AnsweredAssumed Answered

Default frequency bandwidth in ADRF6510

Question asked by Mojea on Apr 25, 2013
Latest reply on Apr 25, 2013 by jdobler

Hello,

 

We are using the ADRF6510 filter in our design as a input filter for a ADC AD9640.

 

We are studing the posibility of use the ADRF6510 controlled only with the Enable input and power.

 

Our question is, after power-up and after the Enable input signal goes to high level, what is the default value of the low pass frequency corner?

 

It is programmed to minimum value 1 MHz or to the maximum of 30 MHz or is not fixed and can be different for each time the power-up is applied.

 

Thank you for your help.

 

Regards.

 

Manuel

Outcomes