AnsweredAssumed Answered

test mp4 encode performance in BF609

Question asked by 921506375@qq.com on Apr 23, 2013
Latest reply on May 7, 2013 by amall

Hi,

I need to boot uClinux and run the uClinux applications in core0 as well as bring up CCES mpeg4 encode applications in core1.If I just use core1 to do mp4 encode,I have no idea if the max output resolution can up to D1 at 30 fps.Is there any way that I can test the mp4 encode performance of core1?Is there any demo that I can use?

Thanks,

lufuyang

Outcomes