AnsweredAssumed Answered

boot Linux on core0 and bring up CCES application on both core0 and core1

Question asked by 921506375@qq.com on Apr 22, 2013
Latest reply on Apr 23, 2013 by Aaronwu

Hi,

I want to test Linux and CCES mcapi interoperability on BF609. I just load BF609_MCAPI_msg_CORE1.dxe to coreb with the command "icc_loader -l BF609_MCAPI_msg_CORE1.dxe"  then run cces_msg1 in linux side and everything is ok. But when I load BF609_MCAPI_msg_CORE0.dxe with the command "icc_loader -l BF609_MCAPI_msg_CORE0.dxe",it says that "

no valid memory region found for 0x0xffa00000

no valid memory region found for 0x0xff900d9c

no valid memory region found for 0x0xff9035a8

no valid memory region found for 0x0xff900000

no valid memory region found for 0x0xff90059c

no valid memory region found for 0x0xff9005d0

no valid memory region found for 0x0xff90305c

writing to 0xc8090000, 0x1a      bytes: OK

writing to 0xc8080420, 0x400     bytes: OK

writing to 0xc809001c, 0x10      bytes: OK

".I wonder if I can boot Linux on core0 and bring up CCES application on botn core0 and core1.

Thanks,

lufuyang

Outcomes