AnsweredAssumed Answered

AD9984 vs ADV7604?

Question asked by FreddyS on Apr 21, 2013
Latest reply on Apr 25, 2013 by joe.triggs

My customer is evaluating solutions for RGB to DVI conversion using the ADV7604 or the AD9984

  1. Is the same core used for AD9984 and ADV7604? 
  2. Dilemma – we want to eliminate picture shift as a result of bad DE generation.
    Is AD9984 or ADV7604 generate proper DE signal? Or it can mimic monitors "Auto adjust" function. 
  3. We want to  use  the same block design for the whole medical product line with different resolution per product. The question is if these
    AFEs are capable to properly digitize esoteric resolutions coming from different equipment ( of course in given BW…) 
  4. PLL- Is it a digital or analog PLL?  Does it need to be programmed for all resolutions independently?


Thanks

Freddy

Outcomes