AnsweredAssumed Answered

WIKI doc for FMCOMMS1 Calibration utility, xcomm_cal, should be updated.

Question asked by jay_d on Apr 16, 2013
Latest reply on Apr 17, 2013 by jay_d

 

The WIKI document for FMCOMMS1 Calibration utility, xcomm_cal, should be updated. The given I2C EEPROM address given is not correct for the xc702 board. I assume the given example is for one of the other Xilinx boards that also works with the FMCOMMS.

It would be very helpful if the WIKI docs for this added some statement as to where the given cal EEPROM is located in the I2C tree for a given board type.

Also the given WIKI doc could add hat the new settings can be listed by typing

grep "" /sys/bus/iio/devices/iio:device4/out_voltage*

grep "" /sys/bus/iio/devices/iio:device5/in_voltage*

 

xcomm_cal docs at  http://wiki.analog.com/resources/tools-software/linux-software/xcomm_cal

 

to note the given FMCOMMS1 cal  eeprom appears at 6-0054 on the xc702

 

Thanks,

James

Outcomes