AnsweredAssumed Answered

ADuM3070 DC-DC Isolated Power

Question asked by Jacky-chen-2 on Apr 15, 2013
Latest reply on Apr 16, 2013 by bkennedy

Dear All:

I would like to planning DC-DC Isolated power solution, need Vin=5V then Vout=5V / Iout=900mA~1A,I try to use EVAL-ADUM3070EBZ 2Pcs to set up my platform. but found that EVAL-ADuM3070 there will be output load are asymmetrical. then I have idea useing ADuM3070 to control 2Pcs transformer JA4631-BL (Pls see below.) this idea is workable? there will be any question? If I need this specification can you provide your suggestion to me refer? or provide available solution to me? thanks

 

 

Best Regards

Jacky

Outcomes