AnsweredAssumed Answered

HDMI and VGA decoding

Question asked by AndyHC on Apr 12, 2013
Latest reply on Apr 15, 2013 by AndyHC

Hi,

 

I have an upcoming project which requires taking in both DVI and VGA video streams (max resolution 1024 x 768), decoding the streams and outputting the resulting data over an IP link. The processor I am planning on using is a Freescale IMx6 Dual which has 2 CSI parallel ports ( up to 20 bit YUV/RGB each). I was planning on using an ADV7611 for the DVI input and an ADV7501 for the VGA input - both devices to be configured for YUV output as this seems to be a native format for the CSI on the IMx6. My question is are these devices sensible choices for my application? if not any advice on suitable devices would be grateful.

 

Regards

Outcomes