AnsweredAssumed Answered

ADG9xx operating on 3.3v VDD supply

Question asked by Laid on Apr 8, 2013
Latest reply on Apr 8, 2013 by Laid

Hello!

 

ADG918 datasheet indicates the power supply requirement between 1.65V and 2.7V. However, at absolute maximum ratings it is specified that the maximum voltage on VDD pin could be up to 4V.

 

Is it therefore safe to run the switch from 3.3V power rail and does it also make the CTRL input compatible with 3.3V logic control signals? Are there any reservations or performance issues if ran on 3.3V power?

 

Thank You and Best Regards,

 

Andrus.

Outcomes