AnsweredAssumed Answered

how to boot the program reside in norflash

Question asked by chenghaibo on Apr 1, 2013
Latest reply on Apr 3, 2013 by chenghaibo

i can debug the program but which can't be booted from the nor flash

 

when set the cess to generate a ldr file, it output two warning message

The artifact type "Loader File" in configuration "Debug" is not applicable to add-in "Startup Code/LDF". The add-in only applies to "Executable" project(s).

 

The artifact type "Loader File" in configuration "Debug" is not applicable to add-in "Pin Multiplexing". The add-in only applies to "Executable" project(s).

 

what 's about the meaning of the warning message and why i can't boot from the nor flash

Attachments

Outcomes