AnsweredAssumed Answered

Updated AD9524 specs and simulation model

Question asked by ak1000 on Mar 27, 2013
Latest reply on Mar 28, 2013 by MFelmlee

Hello,

 

I am using hte AD9524 and noticed that the datasheet was revised in Feb. 2013.  There are a number of changes including the elimination of PLL2 1.8V pin which is now a no connect.  There appears to be a number of page number references that are incorrect under the 2/13 revision.  Without having to go through the entire datasheet, are there any changes I would have to make to my current design besides removing the 1.8V supply to pin 42.  Also, has the simulation model for it been updated as well?

 

Thanks.

Outcomes