rbrennan

ADF4150, ADF4151, ADF4150HV, ADF4152HV evaluation boards software

Discussion created by rbrennan Employee on Mar 27, 2013

The latest ADF4150, ADF4151 and ADF4150HV software (v4) is attached.

 

Installation process:

1. Disconnect any evaluation board

2. Download and run the attached installer

3. Click Next/Continue/Finish when asked

4. Connect your evaluation board

5. Windows will detect the evaluation board and install the drivers

6. Run the ADF4150 Family software from the desktop or Start Menu

7. The status bar of the software should show that the board is connected. If not, try disconnecting and reconnecting the board.

 

Installer includes USB drivers.

 

Reply to this thread if there are any issues.

 

  • v4.4.2: Added warning for maximum MOD value.

Outcomes