AnsweredAssumed Answered

ADV7842 and 480/576i with Component or HDMI inputs

Question asked by adhawkins on Mar 26, 2013
Latest reply on Oct 22, 2015 by pagotici

Hi,

 

I'm trying to send the output from an ADV7842 into the video input port of another processor. Using the SD inputs (e.g. composite) I can successfully transfer PAL and NTSC signals.


However, if I input 480i or 576i via Component YPbPr input, I cannot get correct video capture on the other processor.

 

Can you advise as to what settings I should use for PRIM_MODE and VID_STD in these cases? The documentation suggests that I should switch PRIM_MODE to b0000 (SDP), but if I do this won't I lose the ability to detect the other formats on the Component input?

 

Also, I think I will have similar issues when I put in 1440x576i and 1440x480i via HDMI inputs. In these cases, I still need 720x480 and 720x576 to be passed on to the next processor. Can you advise how to do this?

 

Thanks

 

Andy

Outcomes