AnsweredAssumed Answered

touble to build BF609's mpeg4 demo with CCES

Question asked by 921506375@qq.com on Mar 25, 2013
Latest reply on Apr 5, 2013 by amall

Hi

I just installed the CrossCore Embedded Studio 1.0.1 and MPEG4_SP_ASPEncoder-BF-Rel4.2.0_PROD.exe in order to test BF609's mpeg4 encoder.But when I built the project in the demos,it says " WARN - Add-in "Video Decoder (ADV7842) Driver (1.0.1)" installed in project "mpeg4encbf609_Core0" is NOT found" and "WARN - Add-in "Video Decoder (ADV7842) Class Driver (1.0.1)" installed in project "mpeg4encbf609_Core0" is NOT found". Does it mean that I should install these two drivers first? where can I get thest two drivers and how can I install them?

Thanks

lufuyang

Outcomes