AnsweredAssumed Answered

bf537 SPI Bus: Driver(s) not showing-up in /dev

Question asked by ShutEyeThinkin on Mar 21, 2013
Latest reply on Mar 28, 2013 by ShutEyeThinkin

Using the bf537, I need to install a custom SPI Bus driver.  But it does not show-up in /dev,

even though it is shown to register ok.

 

Also using the SPI Bus is the SPI FLASH chip, which doesn't show the SPI driver, but rather its mtdX's in /dev, and an ad1939 CODEC driver. I see no SPI driver in /dev for the ad1939, either.

 

See attached file for concise info regarding this.

 

Thanks.

Outcomes