AnsweredAssumed Answered

Best full range limiter implementation. - Adau1761

Question asked by Natan on Mar 21, 2013
Latest reply on Apr 10, 2013 by BrettG

I am looking for the "cheapest" in terms of processing resources and memory full range stereo limiter for signals up to +24dB.  The single limiter block is very expensive at 77 instructions\mips  per a channel for a stereo application.  Would the block in:

Dynamic Processors > RMS > Standard Resolution > Full Range (-90 to +24 dB) > No Post Gain > Stereo > No Ext Detector Input > RMS (no gain)

 

perform as well as the limiter block? I appreciate any help.

Attachments

Outcomes