AnsweredAssumed Answered

AD2S1200 Noise Problem

Question asked by fpga_eng on Mar 19, 2013
Latest reply on Mar 21, 2013 by ShaneO

I am using a resolver on a 10 kW motor via the AD2S1200. The DOS and LOT signals indicate a fault after only approximately 10 ms of operation. There is noise being picked up (as seen on the sin, sin_lo, cos, and cos_lo signals) even though screened cables connected to REFOUT are being used. Is it possible to include a filter on the sin, sin_lo, cos, and cos_lo lines just before the AD2S1200 to filter out the noise? If, so could you suggest a circuit. The noise spikes are about 1 microsecond in width.

Outcomes