AnsweredAssumed Answered

AD-FMCOMMS1-EBZ  No OS Ref Design - Waveform Output BarkerCode?

Question asked by DrTom on Mar 18, 2013
Latest reply on Apr 1, 2013 by mhennerich

I have a router set for 802.11b [Channel 1, 1Mbps(max)]  cabled to the input of the AD-COMMS1. I chipscope set to trigger when the value of one of the channels is greater than 0x0100. What I expected to see was DBPSK encoding but I think I am seeing DQPSK because there are two distinct I & Q waveforms, sometimes they are in-phase and other times they are 180 out. I also DO NOT  understand why the I and Q channels seem to decay. The I-Channel will decay to almost zero and then build back up and then the Q-Channel will decay and build back up.

Can anyone explain this?

Thanks...Tom

 

 

 

 

 

 

Outcomes