AnsweredAssumed Answered

Problem with Flashing LDR file to serial Flash using CCES in ADSP21488

Question asked by MZC on Mar 12, 2013
Latest reply on Mar 13, 2013 by CraigG

Hello,

 

I m using the program described in EE355 to flash LDR file. The program is is designed with Visual DSP so i modified the program to use in CCES. With modified program, i am able to correctly flash the LDR file of 28 KB to serial flash But as the size of LDR grows   (i.e 33KB for my case), the pointer to the LDR contents give random wrong values. I used M25P16 serial flash which can store total bytes of 2MB and also used SDRAM and configure these options as described in EE 355 note for ADSP214x.

 

Any idea will be helpful?

 

Best Regards,

 

Mussab

Outcomes