AnsweredAssumed Answered

Use project FPGA reference design for AD9747

Question asked by sergeye34 on Mar 11, 2013
Latest reply on Aug 5, 2015 by CsomI

Hello,

 

I would like to use your project reference design for AD9747 for generating input data.

http://wiki.analog.com/resources/fpga/xilinx/interposer/ad9747

 

I would be grateful if you help to deal with this project.

Is it true that the project can use two modes of formation of the output?

One mode is the DDS.This mode is selected by command “dac dds setup(45MHz, 29MHz)” UART terminal.

http://wiki.analog.com/_media/resources/fpga/xilinx/interposer/cf_ad9747_ebz_uart.jpg

The second mode is the formation of the output data from the memory. How can I use this second mode?

Outcomes