AnsweredAssumed Answered

The ADRF6704 Debug Advisory and get help

Question asked by success@guet.edu.cn on Mar 10, 2013
Latest reply on Mar 13, 2013 by success@guet.edu.cn
  1. Hello.

    I've ADRF6704 the evaluation board circuit  embedded in my project.

 

 

I installed this software ADRF6x0x_customer_6p1p0.



I use the EZ-USB-Interface software download ADRF6x0x_6p1p0.hex.



But I encountered a problem.

My system is WIN7.

 

 

 

 

 

Under “Computer Management \ Device
Manager
\ Universal Serial
Bus Controller|”

 

 

can not display the
correct
hardware drivers,

but is CypressEZ-USB FX2LP-EEPROM missing.

 

 

 

 

 

But "ADRF6x0x eval
board connected" is displayed
inAnakig Devices ADRF6x0x Customer Evaluation Software v6.1.0-ADRF6704
TxMod 2500-2900MHz”
interface .

 

 



May I ask what is the reason?

 

 

 

 

 

Since I design careless,

The 68013A's pins for PA2 --- DATA,
PA1--CLK.,

I want to be able to get the firmware source codes

To modify the control program, this does not change the hardware circuit.

My project PDF file  is attached.




I would appreciate if help soon.

Attachments

Outcomes